Issue
The purpose of this Resolution is to inform users of the 170ADI34000, a 16 point - 24vdc input module, that the 984LL Exec Data Mapping diagram in the Momentum IO Base User Guide is incorrect.
Product Line
Momentum
170ADI34000
Environment
Resolution
The incorrect diagram is found in the 'Momentum I/O Base User Guide', part number 870USE00200, dated 2/2007 and earlier and affects only the 170ADI34000 984LL Data Mapping diagram. It is scheduled to be corrected in a December 2007 Momentum IO Base User Guide release. The IEC Data Mapping diagram for the 170ADI34000 is correct.
This diagram shows the incorrect data mapping pinout in the User Guide
This daigram shows the correct data mapping pinout.
게시 대상:슈나이더 일렉트릭 Korea