FAQ 검색
Do the inputs of the Momentum 170AAI52040 have to be scaled from raw value to an actual temperature value ?
Issue
Do the inputs of the Momentum 170AAI52040 have to be scaled from a raw value to an actual temperature value?
Is a conversion required?
Product Line
Modicon Momentum I/O modules
Resolution
No, this module will provide the actual temperature in units of 1/10 of degrees C or F depending on its configuration.
Therefore, the value simply has to be divided by 10 to get actual temperature in degrees Celsius or Fahrenheit.
게시 대상:슈나이더 일렉트릭 Korea
자세히 알아보기
제품군
자세히 알아보기
제품군