FAQ 검색
Size of the XVDC03 to XVDC12 items
Goals and Symptoms
Size of the XVDC03 to XVDC12 items
Facts and Changes
XVDC
Causes and Fixes
These screw are M5 thread with a lenght of :
XVDC03 : 109mm
XVDC04 : 172mm
XVDC05 : 253mm
XVDC06 : 298mm
XVDC08 : 361mm
XVDC09 : 277mm
XVDC10 : 340mm
XVDC11 : 403mm
XVDC12 : 466mm
Legacy KB System (APS) Data: RESL198039 V1.0, Originally authored by LaBe on 03/16/2009, Last Edited by LaBe on 03/16/2009
Related ranges: Harmony XVD
게시 대상:슈나이더 일렉트릭 Korea
자세히 알아보기
제품군
자세히 알아보기
제품군