Issue
How to change the single user license to a multi-user license on a not yet authorized installation of the
'Advantys Configuration Software'.
Product Line
Advantys Configuration Software version 4.0
Environment
Windows 7
Resolution
Use the following steps to change the the installation from a single user license to a multi-user license
on an unauthorized installation of the Advantys Configuration Software.
- Click on 'Start\All Programs\Schneider Electric\Advantys\Registration' to start the 'Registration Wizard'.
- Click on 'Next'.
- Click on 'Ask for an Authorization Code'.
- Click on the desired method to use for getting the authorization. (i.e., phone )
- Fill in the form that appears.
- Enter the part number for the multiple user license (i.e., use STBSPU1130 at the bottom of the form
- Enter the serial number.
- Click on 'Next'
- Call the 'Registration Center'.
- Click on Next'.
- Enter the received code in the 'Received Authorization Code' entry box.
- Click on 'Next' (A confirmation window will get returned.)
- Acknowledge the confirmation window.
- Close the Registration Wizard.
- Click on 'Help\About' from within the 'Advantys Configuration Software', to verify
게시 대상:슈나이더 일렉트릭 Korea