FAQ 검색
What is the meaning of the error 0X4BE in the error log of the 174CEV20040?
Issue
What is the meaning of the error 0X4BE in the error log?
Product Line
ConneXium - Ethernet
Environment
174CEV20040
Resolution
Error 0x4BE (1214 in decimal, or ERROR_INVALID_NETNAME), when returned from the MB+ driver, it indicates that you are trying to talk to a
nonexistent MB+ node. The Ethernet driver and the bridge software do not generate this error code. Check the routing to see if there is a node called out that is not actually on the network.
게시 대상:슈나이더 일렉트릭 Korea
자세히 알아보기
제품군
자세히 알아보기
제품군