1. System requirements for Concept 2.6 SR6:
- x86-based personal computer (Pentium platform recommended)
- Win98, Win2000, or WinNT 4.0 SP3 or higher (Y2K compatibility requires SP5 ), WinXP Pro or Windows Vista Business 32 Bit
- Win95 is no longer qualified. Win3.1x is no longer supported.
- 24 MB application RAM (or higher)
- CD-Rom drive
- 150 MB hard disk space
- VGA graphics adapter and screen (minimum resolution: 800x600)
- Microsoft compatible mouse
Concept 2.6 SR6 does not support Windows 7 Professional (32). You would need to upgrade to Concept 2.6 SR7 to run on Windows 7 (32)
게시 대상:슈나이더 일렉트릭 Korea