FAQ 검색
Solution of light indication for 400V to 600VAC application ?
Goals and Symptoms
Solution of light indication for 400V to 600VAC application ?
Facts and Changes
LED blocks
Pilot lights
400V
600V
Causes and Fixes
For 440V application, you can use transformer blocks for 24V LED blocks, that will be implemented being the first row of contacts and Led.
400V => ZBV5B
440V - 460V => ZBV8B
550V - 600V => ZBV9B
Legacy KB System (APS) Data: RESL203836 V1.0, Originally authored by LaBe on 12/30/2010, Last Edited by LaBe on 12/30/2010
Related ranges: Harmony XB4
게시 대상:슈나이더 일렉트릭 Korea
자세히 알아보기
제품군
자세히 알아보기
제품군