Product Line
CM100/200 series meter
Environment
Communication Setup
Resolution
Follow the steps below to set the address and baud rate.
- Disconnect control power from the unit
- Set the 2 rotary selector dials to the correct setting for the baud rate (97=9600).
Switch Setting | Baud Rate |
94 | 1200 |
95 | 2400 |
96 | 4800 |
97 | 9600(default) |
98 | 19.2K |
- Restore power
- Wait 5 seconds, disconnect power again
- Set the 2 dials to the desired address (Range includes 1 to 32)
- Restore power.
게시 대상:슈나이더 일렉트릭 Korea