FAQ 검색
Is there a command available to remotely pause the EGX300?
Issue
Can the EGX300 be paused/stopped, temporarily, from updating its webpages and monitoring?
Product Line
EGX300
Environment
Webserver
Cause
This may be desirable, for instance, when a PLC needs to access for a read request.
Resolution
There is no command to temporarily stop the EGX from monitoring. However, if you navigate away from the monitoring pages, it will stop the EGX page communications to the slaves.
게시 대상:슈나이더 일렉트릭 Korea
자세히 알아보기
제품군
자세히 알아보기
제품군