Issue
The purpose of this resolution is to inform 170ENT11001 Ethernet Communication Adapter product users of an issue when assigning an IP address to a 170ENT11001 using Bootp 802.3 Framing.
A problem has existed with the 170ENT11001 in Exec. versions 1.04 and lower where the IP address could not be assigned via Bootp or DHCP when using 802.3 Framing.
Product Line
170ENT11001
Resolution
Assigning an IP via DHCP using 802.3 Framing will not be fixed.
Changes to the Operating System files would be required but they are no longer supported by the vendor.
게시 대상:슈나이더 일렉트릭 Korea