Issue
A customer needs to replace an ION73XX remote display cable.
Product Line
ION73XX Series
Environment
Remote display cable
Resolution
We do not have a pinout diagram for the previously offered RMD cable (DB-25 male to DB-25 female).
Old obsolete part number: 13300-0004
The standard cable shipped with all 73XX remote display optioned meters is a parallel (straight-through) DB25 male/female cable with either a 24 or a 26 wire gauge. The customer can find a replacement cable from a distributor that meets these specs, as we no longer offer this cable. Please ensure the replacement is not 28 gauge as this will fail and cause the remote display to continuously reset or flash.
게시 대상:슈나이더 일렉트릭 Korea