Issue:
Information on the ATS48 Enclosed Soft Start
Product Line:
863948U and 863848U
Environment:
All
Cause:
Instruction bulletin required for the soft start
Resolution:
Please refer to the Altistart 48 Enclosed Soft Start Controllers manual document attachment below. It is document 30072-450-62.
https://www.se.com/us/en/download/document/30072-450-62/
Other related publications:
ATS48 User Manual,
https://www.se.com/ww/en/download/document/1494409/
ATS48 Maintenance & Repair manual, 30072-451-28
https://www.se.com/us/en/download/document/30072-451-28/
게시 대상:슈나이더 일렉트릭 Korea