Issue:
Clearnace issues may create need to know how much space is available between the front mounting rails and the front door.
Product Line:
NetShelter WX
Environment:
AR100 and AR100HD, all serial ranges.
Cause:
The space between the mounting rails and front door in the NetShelter WX is needed for clearance questions.
Resolution:
With the front mounting rails in their forward position as shipped from the factory there's approx. 3" of space available from the mounting rails to the front door.
게시 대상:슈나이더 일렉트릭 Korea