Can M241/M218/M238/M221 PTO only use one output, and another PTO output be used as normal output?No, for M241/M218/M238/M221, one PTO channel must use two outputs! Any PTO output can not be used as normal output when PTO is configured!
게시 대상:슈나이더 일렉트릭 Korea