Issue:
Fault Code Information for the ATV12/212 Drives.
Product Line:
ATV21
Altivar 21
ATV212
Altivar 212
S-Flex
Environment:
All serial numbers for ATV21/212 Drives
Cause:
N/A
Resolution:
Information for the ATV21/212 drive can be found in the programming manual for the drive.
ATV21 Programming Manual is available for download here: https://www.se.com/ww/en/download/document/AAV75193/
ATV212 Programming Manual is available for download here: https://www.se.com/ww/en/download/document/S1A53838/
게시 대상:슈나이더 일렉트릭 Korea