Maximum pulse length depends on the chosen clock frequency:
Clock Frequency | Maximum Size of Pulse |
---|---|
48 MHz | 1.3653125 ms |
24 MHz | 2.730625 ms |
12 MHz | 5.46125 ms |
6 MHz | 10.9225 ms |
3 MHz | 21.845 ms |
1.5 MHz | 43.69 ms |
0.75 MHz | 87.38 ms |
0.375 MHz | 174.76 ms |
0.185 MHz | 354.2432432 ms |
게시 대상:슈나이더 일렉트릭 Korea