If a Base is still linked to a Remote, is it possible to pair it to a another Remote
To link a new Remote to the Base station, the Base station shall be powered OFF before and the pairing shall be done in less than 5 minutes after the power ON of the base station