undefined [object Object]
{}

브랜드

슈나이더 일렉트릭 코리아 웹사이트에 방문해 주셔서 감사합니다.

슈나이더 일렉트릭 코리아 웹사이트 방문자 분들 모두 환영합니다.
오늘 무엇을 도와드릴까요?
How does a MiCOM P63x relay calculate Idiff and Irestrain
Issue
The user would like to calculate the Idiff (differential current) and Ires (restrain current) given the injection currents and matching factors

Product Line
Micom P63x transformer differential relay

Environment
Calculating MiCOM settings

Resolution
The formula below is used by the relay to calculate the Idiff and Irestrain:
Calculation of the differential and restraining currents
To simplify the equations, assume that the Zero-sequence current filtering is disabled :

  Zero-sequence current filtering
 
Where Kam,a and Kam,b are the amplitude matching factors calculated by the relay based on Iref/Inom on side a and side b, respectively. Refer to the differential protection section in the manual for more information.
 
Example:
I,a,sec = 10 A                     I,nom,secondary= 5 Amps             Kam,a= 2.76
I,b,sec = 5 A (180 deg)        Kam,b= 1.32
 
Formula for example
 
Iref is calculated based reference power and the nominal voltage on side a and b.