FAQ 검색
What is the communications cable between the Magelis XBTN200 / XBTN400 and Modicon M221 controller?
Issue:
What is the communication cable needed between an M221 and XBTN.
Product Line:
M221
XBTN200
XBTN400
Resolution:
Tthe communications cable between the XBTN400 and M221 is XBTZ9980
This is a Modbus RS485 communication cable.
What is the communication cable needed between an M221 and XBTN.
Product Line:
M221
XBTN200
XBTN400
Resolution:
Tthe communications cable between the XBTN400 and M221 is XBTZ9980
This is a Modbus RS485 communication cable.
게시 대상:슈나이더 일렉트릭 Korea
첨부 파일
자세히 알아보기
제품군
자세히 알아보기
제품군