Issue:
You are using the PowerChute Agent to protect your Windows desktop machine with hibernation and/or sleep enabled and experience communication issues on wake-up.
Product Line:
PowerChute Business Edition 9.1, 9.1.1, 9.2, 9.2.1, 9.5, 10.x
PowerChute Serial Shutdown
Environment:
All supported Windows OS
Cause:
When connected to a Smart-UPS or Easy-UPS, hibernate and Sleep are not supported with PowerChute Business Edition or PowerChute Serial Shutdown.
Hibernate is supported when PowerChute Serial Shutdown is connected to a Back-UPS starting with version 1.2
Solution:
Disable Hibernate and or Sleep for shutdown in Power Options
게시 대상:슈나이더 일렉트릭 Korea