Issue
Number of MAC addresses on a M580 CPU
Product Line
M580 PAC
Environment
Unity Pro or Control Expert
Resolution
Each M580 CPU has 3 MAC Addresses. But only 1 MAC address, which is the Service port MAC address, is silk screened on the CPU Module and is associated with the Unity program assigned IP address.
The other MAC addresses are required for the other two physical Ethernet ports. Each physical Ethernet port is required to be assigned a unique MAC address.
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
게시 대상:슈나이더 일렉트릭 Korea