undefined undefined
{}

브랜드

슈나이더 일렉트릭 코리아 웹사이트에 방문해 주셔서 감사합니다.

슈나이더 일렉트릭 코리아 웹사이트 방문자 분들 모두 환영합니다.
오늘 무엇을 도와드릴까요?
What is the resistance against the material of the reference ZBDD2 ?
Its material is polyurethane (PU), its material has a good resistance against the UV.

By the way its cap is sold in the harsh environment catalogue that means it is done to be used in industrial machines which can go outside and in marine, applications where UV are present.

슈나이더 일렉트릭 Korea

What is the resistance against the material of the reference ZBDD2 ?
Its material is polyurethane (PU), its material has a good resistance against the UV.

By the way its cap is sold in the harsh environment catalogue that means it is done to be used in industrial machines which can go outside and in marine, applications where UV are present.