Issue:
BRH parameter meaning in Somove.
Product Line:
ATV71 drives
Environment:
All
Cause:
BRH appears in the Somove software but does not show up in the drives parameters.
Resolution:
BRH on somove is the setting word of BRHB0, BFRHB1, BRHB3, with for example BRHB0=1 and BRH3=1 the, BRH=5.
BRH parameter meaning in Somove.
Product Line:
ATV71 drives
Environment:
All
Cause:
BRH appears in the Somove software but does not show up in the drives parameters.
Resolution:
BRH on somove is the setting word of BRHB0, BFRHB1, BRHB3, with for example BRHB0=1 and BRH3=1 the, BRH=5.
게시 대상:슈나이더 일렉트릭 Korea