FAQ 검색
Video: What is the difference between Model 6 Standard and Industrial MCC's?
Both the Standard and Industrial MCC can be ordered in enclosure types NE MA 1, 1 A, 12 or 3 R. The Standard package lets you tailor the MCC by selecting only the options needed for an individual project, providing optimal cost / value balance. The Industrial package includes options most commonly requested and specified for industrial customers. Offering the options as part of a package reduces the possibility of leaving out common industrial features. This list represents the comparison of the two packages.
(1) Exceptions: 1600-3200 Amp are Tin-plated Copper
(2) Structure Premium Barrier System; formerly Fish tape Barriers
(3) Unit Fish tape Plugs are not required when Premium Barrier System is provided
Structure Feature | Standard Package | Industrial Package |
Vertical Ground Bus Material | Steel | Copper |
Horizontal Bus Material | Tin-plated Aluminum (1) | Tin-plated Copper |
Premium Barrier System (2) | Optional | Optional |
Unit Feature | Standard Package | Industrial Package |
Unit Fish tape Plugs (3) | Optional | Included |
Interior Color | Gray | White |
Nameplates | Optional | Included |
X 1 and X 2 wired to terminal blocks | Optional | Included |
(2) Structure Premium Barrier System; formerly Fish tape Barriers
(3) Unit Fish tape Plugs are not required when Premium Barrier System is provided
게시 대상:슈나이더 일렉트릭 Korea
자세히 알아보기
제품군
자세히 알아보기
제품군