Issue
Customer would like configure a Vista grouping object to open the correct meter diagram.
Product Line
ION Enterprise 5.6, 6.x
Struxureware Power Monitoring 7.x
Power Monitoring Expert 8.x
Environment
Vista
Resolution
YouTube
Customer would like configure a Vista grouping object to open the correct meter diagram.
Product Line
ION Enterprise 5.6, 6.x
Struxureware Power Monitoring 7.x
Power Monitoring Expert 8.x
Environment
Vista
Resolution
- Right-click on the grouping object to open the Grouping Object Configuration window
- Specify Node
- Select the Node tab

- Select Custom and navigate to the desired meter.
- (Optional) Specify the grouping object image
- In the Display tab, select Custom
- Select the desired image. Images of native devices are located in \Power Monitoring Expert\config\diagrams\images\default
- Specify the Action
- In the Action tab, select Open Diagram for Meter Template
- Press OK
- Press Save to save the changes
- Double-click on the grouping object to verify the grouping object functions properly
게시 대상:슈나이더 일렉트릭 Korea