Issue:
Perform a factory reset on an ATV320 drive.
Product Line:
Altivar 320, ATV320
Environment:
All
Resolution:
To perform a factory reset from power up;
Enter on dial.
Scroll down to CONF menu and enter.
Scroll down to FCS- and enter.
Scroll down to FRY- and select all if you would like to reset all parameters (including function blocks). The two vertical lines to the right of 'all' should move up.
ESC back to FRY-.
Scroll down to GFS and enter.
Scroll down to yes and enter (hold for 3 seconds).
The parameter GFS should go to NO automatically. This is when you know factory reset has been done.
“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
게시 대상:슈나이더 일렉트릭 Korea