Integrated ARC protection is supported in Easergy P3 Advanced models except for the P3L30 model which do not support ARC protection
Totally 4 sensors can be connected and the sensor is same as the point sensor for dedicated Schneider ARC protection.
Totally 4 sensors can be connected and the sensor is same as the point sensor for dedicated Schneider ARC protection.
게시 대상:슈나이더 일렉트릭 Korea