Issue:
ATV600 or ATV900 wiring comparison to ATV61 or ATV71
Product Line:
ATV630 ATV930 Process Drive
Environment:
All
Cause:
Wiring
Resolution:
DI's (Digital) = LI's (Logic)
AI1 and AI2 are the same as the ATV61/ATV71, except the ATV600/ATV900 do not have AI1- Bi-Polar Input
AO1 from ATV61/ATV71 = AQ1 on ATV630/ATV930 (Analog Output)
DQ + and DQ - are the Digital Outputs on ATV630/ATV930
R1, R2, R3 = Programmable Relays with most of the same functions
ATV600 or ATV900 wiring comparison to ATV61 or ATV71
Product Line:
ATV630 ATV930 Process Drive
Environment:
All
Cause:
Wiring
Resolution:
DI's (Digital) = LI's (Logic)
AI1 and AI2 are the same as the ATV61/ATV71, except the ATV600/ATV900 do not have AI1- Bi-Polar Input
AO1 from ATV61/ATV71 = AQ1 on ATV630/ATV930 (Analog Output)
DQ + and DQ - are the Digital Outputs on ATV630/ATV930
R1, R2, R3 = Programmable Relays with most of the same functions
게시 대상:슈나이더 일렉트릭 Korea