FAQ 검색
What to do if a message with ID 0x1443 or 0x1444 is displayed on the MicroLogic X screen.
These messages are generated by the Circuit Breaker Service Life Monitoring function of the MicroLogic X control unit, to indicate that a predefined number of operations of the circuit breaker is reached.
Refer to the MicroLogic X User Guide:
- For information about the Circuit Breaker Service Life Monitoring function and recommended actions.
- For information about how to acknowledge a message on the MicroLogic X screen
게시 대상:슈나이더 일렉트릭 Korea
자세히 알아보기
제품군
자세히 알아보기
제품군