FAQ 검색
What is the maximum number of ASi modules supported by the M580 PLC platform ?
Issue:
Max number of ASi modules supported by the M580
Product Line:
EcoStruxure Control Expert, BMXEIA0100
Resolution:
The following maximum number of AS-i modules on a local rack containing one of the following CPUs is allowed.
Max number of ASi modules supported by the M580
Product Line:
EcoStruxure Control Expert, BMXEIA0100
Resolution:
The following maximum number of AS-i modules on a local rack containing one of the following CPUs is allowed.
- BMEP581020: 2 modules
- BMEP582020: 4 modules
- BMEP582040: 4 modules
- BMEP583020: 6 modules
- BMEP583040: 6 modules
- BMEP584020: 8 modules
- BMEP584040: 8 modules
- BMEP585040: 8 modules
- BMEP586040: 8 modules
게시 대상:슈나이더 일렉트릭 Korea
자세히 알아보기
제품군
자세히 알아보기
제품군