To properly reset to factory the switch you will need :
Then proceed as follows
- a Modicon Memory Back Up Adaptor with the reference MCSEAM0100
- a USB type C cable
- Power off the switch
- From your PC put an empty 'recovery.txt' file on the Modicon Memory Back Up Adaptor
- Eject the Modicon Memory Back Up Adaptor safely from your PC via the Windows menu
- Plug the Modicon Memory Back Up Adaptor into the switch
- Power up the switch
- Wait for the status LED to start flashing
- Remove the Modicon Memory Back Up Adaptor
- Plug in the USB type C cable connected to your PC
- Open the terminal window ( through Putty emulator for instance)
Then proceed as follows
- Change from the main menu to Manage configurations : press the <4> key
- Execute the Clear configuration and boot param command : press <1> key
- To load the factory settings : press the <Enter> key
- To go back to main menu : press <q> key
- To reboot the device with factory settings : press the <q> key
게시 대상:슈나이더 일렉트릭 Korea