It’s important to know the following information when there is problem on the OPCUA protocol between the OPCUA client and the OPCUA Server:
We need to know:
We need to know:
- Simple architecture of the whole system between OPCUA Client and Server and other Network connection
- OPCUA Client: which SCADA, what is the OPCUA Stack (From OPC Foundation, Unified automation, …), How it is developped the OPCUA client (C#...)?
- Subscription setting:
- LifeTimeCount configured from OPCUA client
- Publishing Interval configured from OPCUA client
- Session Timeout configured from OPCUA client
- Monitored Item Setting
- Sampling Interval configured from OPCUA client
- Mast Cycle time of the PLC
- Subscription setting:
- Monitored Item Setting
게시 대상:슈나이더 일렉트릭 Korea