Issue:
How to online M340 via BMXNOM0200 through ModbusTCP gateway in Control Expert ?
Product Line:
M340
Environment:
EcoStruxure Control Expert
Resolution:
The address syntax could be expressed as ModbusTCP_Gateway_IP;BMXNOM0200_slave_number
In this sample, the 192.168.10.20 is the IP address of ModbusTCP_Gateway, which could be accessed by the PC where the control expert is installed. One channel of BMXNOM0200 should be configured as a Modbus slave with address 1 and it should be wired to the Modbus link of the ModbusTCP gateway.
게시 대상:슈나이더 일렉트릭 Korea