FAQ 검색
Are there any settings needed to run a ATS22 soft start on a Corner Grounded Delta System?
Issue:
Settings needed to run a ATS22 soft start on a Corner Grounded Delta System.
Product Line:
ATS22
Environment:
Corner-Grounded Delta system
Cause:
n/a
Resolution:
When you have a corner grounded system on the ATS22, DO NOT change the DETLA settings in the config menu, leave it as LINE.
Would also suggest to go CONF menu and set LAC to on and then go to the ADJ menu and turn the SSC to off.
게시 대상:슈나이더 일렉트릭 Korea
자세히 알아보기
제품군
자세히 알아보기
제품군