Issue:
Need to have a specific panel or page to be displayed on the HMI when it wakes up and the backlight turns ON.
Product Line:
Vijeo Designer, Magelis HMI and Harmony HMI.
Resolution:
The information for the HMI backlight status and control can be found in the Vijeo Designer Help, section 6.7.1:
To have the HMI go to a specific panel when it wakes up and the backlight comes ON, follow these steps:
Set the Backlight - Sleep after property of the target under the Hardware tab.
Then configure a Conditional Action using the trigger variable "_BackLight.Status", trigger "On Data Change" and click Next.
Add a Decision operation on the "_BackLight.Status" system variable, that when true, will do a Change Panel action to the desired panel.
Then, click the Finish button. Make sure the action is added correctly.
See the Test_Backlight.vdz example project.
게시 대상:슈나이더 일렉트릭 Korea