How will the peak controller or connection to TIC (France only) avoid the incoming circuit breaker to trip ?EVlink Home reduces the power then stops the charge when it remains only 6A available and it will restart when there is 8A available.
게시 대상:슈나이더 일렉트릭 Korea