Issue:
What is the DHCP name of BMENOS0300 located in remote rack ?
Product Line:
M580
Environment:
EcoStruxure Control Expert
Resolution:
The DHCP name of BMENOS0300 is expressed as Cxxx_0y_BMENOS.
C002_06_BMENOS means it is loacted in the seventh slot (06) of a remote rack identified as CRA has rotary address 2
C105_04_BMENOS means it is loacted in the seventh slot (04) of a remote rack identified as CRA has rotary address 105