The WebVisualization of EcoStruxure Machine Expert can display videos by following these steps:
1) Create a new .html file. (Simply create a normal .txt file and rename the .txt extension to .html)
2) Copy the following content into the file and paste the filename of the video
<html> <video controls="true" height="480" width="640"> <source src="video.mp4" type="video/mp4" /> </video> </html>
3) Transfer the .mp4 and the .html file to the controller (under the folder visu). Important: The two files must be in the same directory.
4) Start the controller and open the webpage http: // <IP-Address>: 8080 / <Your HTML file name> .html or http: // <IP-Address>: 8080 / <Folder name> / <Your HTML file name> .html
Note:
The html file can be accessed directly via the link. It is not managed by the device user rights management.
게시 대상:슈나이더 일렉트릭 Korea