{}

브랜드

슈나이더 일렉트릭 코리아 웹사이트에 방문해 주셔서 감사합니다.

슈나이더 일렉트릭 코리아 웹사이트 방문자 분들 모두 환영합니다.
FAQ 검색
Does the M340 Can-Open master detects the presence of the devices which are not configured?
The answer is yes:
This behavior is part of the bootup procedure specified in the standard "CiA302".
At the end of the bootup procedure, after all expected slaves have got their configuration data, a "start all nodes" command is sent by the master.
So each devices connected to the network are identified.

슈나이더 일렉트릭 Korea

Does the M340 Can-Open master detects the presence of the devices which are not configured?
The answer is yes:
This behavior is part of the bootup procedure specified in the standard "CiA302".
At the end of the bootup procedure, after all expected slaves have got their configuration data, a "start all nodes" command is sent by the master.
So each devices connected to the network are identified.