{}

브랜드

슈나이더 일렉트릭 코리아 웹사이트에 방문해 주셔서 감사합니다.

슈나이더 일렉트릭 코리아 웹사이트 방문자 분들 모두 환영합니다.
오늘 무엇을 도와드릴까요?
What is the maximum number of connections the BMENUA0100 module can open to the M580 CPU?
Issue:
Maximum number of connections the BMENUA0100 module can open to the M580 CPU


Product Line:
BMENUA0100


Resolution:
The number of connections the BMENUA0100 module can open to the M580 CPU depends on the capacity of the CPU. Thus, performance of the BMENUA0100 module will depend on the time required to perform the MAST task and the selected CPU. The maximum number of connections opened by each BMENUA0100 module to the M580 CPU are as follows:

image1

슈나이더 일렉트릭 Korea

What is the maximum number of connections the BMENUA0100 module can open to the M580 CPU?
Issue: 
Maximum number of connections the BMENUA0100 module can open to the M580 CPU


Product Line:
BMENUA0100


Resolution:
The number of connections the BMENUA0100 module can open to the M580 CPU depends on the capacity of the CPU. Thus, performance of the BMENUA0100 module will depend on the time required to perform the MAST task and the selected CPU. The maximum number of connections opened by each BMENUA0100 module to the M580 CPU are as follows:

image1