{}

Наши бренды

Impact-Company-Logo-English Black-01-177x54

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
Поиск часто задаваемых вопросов
What is the bandwidth of the skip frequency, JPF on the ATV12 drive?
Issue:
Bandwidth of the skip frequency, JPF on the ATV12 drive.

Product Line:
Altivar ATV12

Environment:
All serial numbers

Cause:
N/A

Resolution:
The bandwidth is +/- 1 Hz around the JPF setting.  Example, JPF = 30, the drive will not run at speeds between 29 Hz and 31 Hz.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Казахстан

Узнайте больше
Линейка:
Статьи, которые могут оказаться полезными
Узнайте больше
Линейка: