{}

Наши бренды

Impact-Company-Logo-English Black-01-177x54

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.

Поиск часто задаваемых вопросов

How do I update the “Date of last Battery Replacement” seen in NMC card GUI?

Issue:
How do I update the “Date of last Battery Replacement” seen in NMC card GUI?

Product line:

Smart-UPS VT, Galaxy 3500, Symmetra PX1

Environment:
All models, all serial numbers

Cause:
The system does not automatically update battery age / replacement information, it must be manually changed whenever all of the batteries are replaced.

Resolution:

Log into the NMC web interface click on the UPS tab then under the Configuration section is the option for General, select General and you will see the options for “last battery replacement”
1

And

2

Update when all batteries have been replaced.
Note, This only applies to units running FW 5x or lower

Schneider Electric Казахстан

Узнайте больше
Линейка:
Galaxy 3500Smart-UPS VTUPS Network Management CardsSymmetra PX
Узнайте больше
Линейка:
Galaxy 3500Smart-UPS VTUPS Network Management CardsSymmetra PX