Issue:
Motor runs wrong direction in AFC
Product Line:
ATV212, SFLEX
Environment:
All models
Cause:
None
Resolution:
Recommendation , swap two of the drive output leads T1-T2-T3 (motor leads). Swap the leads between the drive output terminals (load side) and drive output contactor (line side).
Опубликовано для:Schneider Electric Казахстан