Goals and Symptoms
Is it possible to open the SFT 2841 with all the connection parameters already defined ? In other words, one wants to start the SFT 2841 from under their SCADA and the have the SFT 2841 software automatically connect to a given Sepam unit (without inserting manually the connection parameters like IP address of the gateway and Sepam Modbus address)
Causes and Fixes
It is not possible . You do need to set network configuration in SFT2841, before being able to get distant connection via IP address
Re-published to revised security level: 17 June 2008 by DRM
Applies To: SFT2841
Public
All content © 1992-2008 Schneider Electric
Legacy KB System (APS) Data: RESL177774 V2.0, Originally authored by KBAdPM on 11/05/2007, Last Edited by DaMi on 06/18/2008
Related ranges: SFT 2841 - SFT2848 (Sepam series 20, 40, 80 software)
Опубликовано для:Schneider Electric Казахстан