Поиск часто задаваемых вопросов
What is the default password of the SEPAM relay?
Issue
Don't know the password to make changes to the SEPAM relay.
Product Line
SEPAM 20, 40, 60, and 80 Series
Environment
Modifications to settings or events
Resolution
The default password is "0000". This is a 2 key password that allows the operator to access and change all data, including protection settings and SEPAM parameter settings. The operator will also be able to clear/reset alarms and peak values.
If the password was changed or has been forgotten, please contact our Technical Support team at 888-797-6468 Option 3, email:usenergyts@schneider-electric.com.
Опубликовано для:Schneider Electric Казахстан
Узнайте больше
Линейка:
Узнайте больше
Линейка: