Title
MiCOM S1 Studio - Getting Started Guide
Issue
Documentation required
Product Line
MiCOM relays
Environment
Easergy Studio (MiCOM S1 Studio)
Resolution
MiCOM S1 Studio - Getting Started Guide provides a user-friendly, simple approach to learning the basics of using Easergy Studio (MiCOM S1 Studio). Some features include:
- Create a New System
- Open an Existing System
- Export a system
- Import a System
- Copy/Paste an Element
- Delete an Element
- Move an Element
- Add a Device
- Add a Substation, Voltage Level, or Bay
- Quick Default Settings File Guide
- Open a Settings File
- Send Settings to a Device
- Compare Settings Files
- Quick Access Control Guide
- Quick Connection Guide
- Use Predefined Connections
- Make a Default Connection
This document does not provide details on how to retrieve Data Models using the Data Model Manager. For that, refer to the following Knowledge Base articles:
Video: How to add a Data Model to Easergy Studio (MiCOM S1 Studio)
Video: How to export data models for MiCOM relays
Video: How to Import MiCOM Data Models
Опубликовано для:Schneider Electric Казахстан