Поиск часто задаваемых вопросов
What are the part numbers of the connection cable between Magelis XBTGH2460 and XBTZGJBOX junction box?
Issue:
Part numbers for the connection cable between Magelis XBTGH2460 and XBTZGJBOX junction box
Product Line:
XBTGH2460, XBTZGJBOX
Resolution:
The connection cable part numbers between the Magelis XBTGH2460 and XBTZGJBOX junction box are:
XBTZGHL3 (3 meter cable)
XBTZGHL10 (10 meter cable)
XBTZGHL20 (20 meter cable)
Опубликовано для:Schneider Electric Казахстан
Узнайте больше
Линейка:
Узнайте больше
Линейка: