Issue
How to configure the STBEHC3020 for modulo mode.
Product Line
All versions of the Advantys Configuration Software.
Environment
Windows 7
Resolution
Connect the 'STBEHC3020' to the incremental encoder and configure the parameters in the Advantys Configuration software using the following instructions:.
- Double click on the 'STBEHC3020' module to open the properties window for the module.
· Configure the parameters as shown.
· Download the application to the island.
· Start the PLC.
· Place the PLC into test mode.
Set the Input Validation bits to Off.
Set the Counter Enable to On.
Set the Counter Sync bit to On.
To reset the counter, toggle the counter sync bit from 0 to 1.
Опубликовано для:Schneider Electric Казахстан