Product
ION Setup
Issue
When a user tries to use the Setup Assistant in ION Setup to change the scaling of a DNP measurement from custom to a fixed value (e.g. 0.01), an error window might pop-up saying: "Configuration requires too many modules; requires 22 , maximum 20".
Cause
This is a known bug of the DNP configuration in the Setup Assistant wizard.
Resolution
Restarting ION Setup generally resolves this issue, but another way to configure DNP scaling is to use the advanced mode of ION Setup and configure the DNP modules manually.