What is the correct setting of the two contact thermometer temperature thresholds of Oil Distribution Transformers?
The correct setting of the two contact thermometer temperature thresholds of Oil Distribution Transformers is maximum 85°C for alarm and 95°C for tripping, although lower temperatures might be set by the user.